AXIS#.SM.ACC

Description

Sets the acceleration ramp for service motion.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

See Acceleration Units for details.

Range

Depends on units. See Acceleration Units for details.

Default Value

30,000 rpm/s

Depends on units. See Acceleration Units for details.

Data Type

Float

See Also

Service Motion
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
AXIS1.SM.ACC

500eh

08h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.SM.ACC

510eh

08h

Unsigned32

Acceleration

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.SM.ACC

6408

1908

Unsigned32

Read/Write

Acceleration

AXIS2.SM.ACC

71944

1190

Unsigned32

Read/Write

Acceleration

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.SM.ACC

6408

Float

Read/Write

Acceleration